Other Parts Discussed in Thread: HDC3020
Hello Team,
I want to check with you about 2 HDC3022 configuration issue from my customer. Thanks.
1. When they use 0x61bb command configure 0x03b013, we see that the device isn't working. Using 0xE001 and 0xE002 command read data, data is abnormal and the CRC is also incorrect.
The customer requirement is to set the HDC3022 to go to auto-measurement mode after power on or reset, measure 1 time in 2 seconds(0x30b0). And the Alert Pin should be triggered by the customer configured threshold. Can you share the register sequence to meet the customer requirement?
2. During verification, they are using trigger measurement mode, we see that the 1st time measure after power on is always incorrect, read data is all 0 except for CRC. And the 2nd time measured data is the 1st time measure data. In this status, we didn't see NACK. In the D/S, we say that when measurement not correctly, there should be NACK bit. Is this behavior normal?
Thanks!
Regards,
Qiang