Hello,
I have the following questions regarding the single-byte read of TMP422:
- If I want to do a single-byte read for all the three temperature registers: Local Temperature Reg (x"00"), Remote Temperature Reg 1 (x"01"), and Remote Temperature Reg 2 (x"02"), does the master has to Start the data transfer, then stop it for each register?
- Or can the master only issue one start data transfer, and after received the data from Remote Reg 2, issue the stop data transfer?
Best regards,
Mark