This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMP422: Single-Byte Read

Part Number: TMP422

Hello,

I have the following questions regarding the single-byte read of TMP422:

  1. If I want to do a single-byte read for all the three temperature registers: Local Temperature Reg (x"00"), Remote Temperature Reg 1 (x"01"), and Remote Temperature Reg 2 (x"02"), does the master has to Start the data transfer, then stop it for each register?
  2. Or can the master only issue one start data transfer, and after received the data from Remote Reg 2, issue the stop data transfer?

Best regards,
Mark