Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed from November 25 through December 2. Thank you for your patience.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1443BOOST: IWR1443 + DCA1000EVM: No device information after Uniflash-SFORMAT-Command

Part Number: IWR1443BOOST
Other Parts Discussed in Thread: UNIFLASH, , DCA1000EVM

Hello everybody,

I tried to run the Quick Start Demo for the DCA1000EVM, which is attached to an IWR1443BOOST, but I failed. The most obvious sign for this was the MSS firmware version that was not visible after loading (0.0.0.0). So I read some issues in this forum and the DCA1000 Debugging Handbook, where it is recommended to use UniFlash's SFORMAT function to clear the flash and repeat the process (Quick Start Demo). But after this step, the information about the Device Status, Die Id, BSS and MSS firmware, and patch versions in mmWave Studio 2.1.1.0 are missing. When I press "Set (1)" on the Reset Control section the software crashes and when I press "SPI Connect(5)" an error prompts ("Power on One Device at time").

Please check the attached images (mmWave Studio, hardware and switch settings, UniFlash). Thanks in advance.

.