This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1443BOOST: WR1443BOOST No reply

Part Number: IWR1443BOOST

Dear Sir

Please advise me regarding the following.

I confirmed detection with IWR1443BOOST using mmWave Demo Visualizer.

After that, I sent profile_2d.Cfg (located in mmwave_sdk_02_01_00_04\packages\ti\demo\xwr14xx\mmw\profiles\) using a program written in Python,

but there was no reply. Please give me detailed instructions on how to reply.

I checked the COM port in the device manager and it is correct.

It reads each line from the file, converts it to byte code, and sends it. (Try both with and without \n)

Thank you

H.Imabayashi

  • Hello.

    Have you tried sending your configuration through a serial terminal like tera term to make sure that the configuration is valid and the device is sending data back to the host?  In addition, if you are using your own script to send the CLI, please refer to the applications visualizer in the radar toolbox as a starting point, as that is a python-based gui that also is able to send CLI and receive data from the device.

    Sincerely,

    Santosh