This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1843AOP: mW Power and GPIO variable frequency question

Part Number: AWR1843AOP
Other Parts Discussed in Thread: AWR1843

I have questions about the AWR1843AOP

 

It specifies a transmit output in dB but I am looking for mW. Can you provide? I am trying to meet a <100mW requirement

 

Also for the GPIO, I would like to use a variable frequency output which I can change depending on conditions at a frequency of 10Hz (10 times per second) and vary between 0.1Hz and 6.5kHz

 

Does the 1843AOP have a GPIO which could provide this?

Thank you