Part Number: TMCS1123
Other Parts Discussed in Thread: INA3221, , INA228, AMC131M03, TMCS1100
I was advised to use TMCS1123 to measure alternating current when using TEC controller for peltier cooling. Voltage changes from -15V to +15V or actually polarity of voltage changes depending on heating or cooling. Current stays under 5A. I want to measure also the voltage in addition to current. I was advised to use Texas instrument ADC that also include I2C communication. I have used INA3221 to do this whole thing when polarity does not change but now I have issue with changing polarity and that's why I am forced to use other method. Is this possible?