This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1642BOOST: mmwave_automotive_toolbox_3_6_0 driver vital signs tlv type

Part Number: IWR1642BOOST
Other Parts Discussed in Thread: IWR6843, IWR1642

Hi,

I'm parsing "C:\ti\mmwave_automotive_toolbox_3_6_0\labs\incabinsensing\driver_vital_signs\vitalSigns_host\gui\gui_exe\dataOutput When FromEVM.bin" data format encountered TLV type 00 and 01, I would like to ask what kind of data type is this? As shown below:

The following two pieces of code are from "C:\ti\mmwave_industrial_toolbox_4_12_1\labs\Vital_Signs\68xx_vital_signs\parse", If I want to change the following two pieces of code to change the data types from 06, 02 to 00, 01 what should I do?

Thanks in advance,Looking forward to your reply.

Best regards