This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1843BOOST: I am working with IWR 1843 BOOST for vital signs detection. I have few questions and i need support in working with it.

Part Number: IWR1843BOOST
Other Parts Discussed in Thread: IWR1843, IWR6843, IWRL6432

Hi,

 I am Surya. I am working with IWR 1843 BOOST for vital signs detection. I have few questions and i need support in working with it.

1. Can IWR 1843 BOOST be used for vital signs detection..?

2. If so can you help me in finding the resources required like work flow, how to get the raw data.. and conversion of raw data to adc samples and heatmaps.

Thank you,

Surya.

Research Scholar.

Contact: +91 9701353153

  • Hi Surya,

    1. Vitals signs demo on IWR1843 is no longer supported. You need to use IWR6843 ISK or AOP for Vital signs. Also, Vitals signs demo is available on IWRL6432

    2. You can refer to the vitals signs demo in radar tool box at radar_toolbox_2_00_00_06\source\ti\examples\Medical

    3. If you want to get yourself familiarized with using the IWR1843, you can try running the out of box demo at radar_toolbox_2_00_00_06\source\ti\examples\Out_Of_Box_Demo

    Regards