Hi,
I am designing a medical-grade pH meter that needs to pass the Level 4 ESD test. The pH electrodes have very high internal resistance, so the op amp must have a very low input bias current (the LMP91200 has an input bias current of less than 1 pA). Can you recommend any ESD protection solutions for such applications? I cannot use TVS diodes because most of them have leakage currents greater than 1 nA, which is an order of magnitude higher than the input bias current of the op amp
I am considering placing a large value pulse-withstand resistor (10 MΩ) in series with the input and a 100 pF capacitor to ground. Additionally, I plan to add a low leakage current TVS diode between the guard ring and ground.
I would be very grateful for any advice.