This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPT3001: Schematic Review

Part Number: OPT3001

Tool/software:

Hi,

Customer wants to use MCU's WAKEUP function by receiving INT of OPT3001 sensor.

Please review the schematic review.

  • Hi Cho,

    Please make sure that the customer has pull up resistors for SCL, SDA, and INT. The datasheet recommended value for these pull up resistors is 10 kΩ. Additionally, the INT pin should be connected directly to the MCU. Please refer to the example schematic from the datasheet:

    Best regards,
    Nicole