Part Number: AWR6843AOPEVM
Other Parts Discussed in Thread: MMWAVE-L-SDK, IWRL6432BOOST, IWRL6432, AWR6843
Tool/software:
I recently purchased the AWR6843AOPEVM and I am attempting to run some example projects. My goal is to complete the Video Doorbell project and the Vital Signs project.
After installing Code Composer Studio, I visited the link (https://software-dl.ti.com/ra-processors/esd/MMWAVE-SDK/latest/index_FDS.html) to download and install the MMWAVE-L-SDK for Windows. The downloaded file is named 'MMWAVE_L_SDK_05_04_00_01-Windows-x86-Install.exe'.
Next, I opened CCS Thesia, and in the 'Create New Project' window, I entered AWR6843AOPEVM and selected the Video Doorbell Example. However, when I clicked CREATE, I received the following error message: 'Error: Product MMWAVE-L-SDK v5.4.0.00 is not currently installed and no compatible version is available. Please install this product or a compatible version.'
Despite having installed the SDK, why am I encountering this error? Additionally, when I select 'Vital Signs xWRL64xx AppSS' from the examples and try to create it, I receive the same error message.