Tool/software:
Dear Sir/Madam,
I am currently using the AWR6843AOPEVM for 3D occupancy detection and have encountered the following issue:
When using the default .cfg file, the point cloud distribution is accurate. However, after altering the TX phase shifts in the .cfg file, the point cloud signals corresponding to the objects under test appear to be shifted, even though the experimental setup remains unchanged.
Below is the point cloud generated using the default .cfg file.

Below is the .cfg file after changing the phase shifts.

I would like to confirm if there are any documents or explanations available that describe how changes in phase shift can affect the point cloud algorithm, resulting in the displacement of points representing the objects in the point cloud.
Thank you for your time and support.
Best regards,
Hsiu-Che Chang