This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMP236: Thermal design of TMP235/236 series temperature sensor

Part Number: TMP236
Other Parts Discussed in Thread: TMP235, ISOTMP35

Tool/software:

Dear Friend

My application is to protect a linear Mosfet from overheating with possible heavy/overstressed usage.  the Mosfet is surface mounted with its drain connected to a piece of copper on top of PCB. My plan is to mount the TMP236A2DCKR near the Mosfet with its body glued on the same piece of copper by Kafuter K-5204K Silicone Adhesive Paste.  My questions are:

1. Is my plan good enough for the sensor to sense the true case temperature of the Mosfet?

2. Should/Can I connect pin1 and pin5 of the TMP236 to the same piece of copper?

3. Any other better thermal design in such applications?

 

Best Regards

Tony