This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPT3101: OPT3101 receives amplitude saturation

Part Number: OPT3101


Tool/software:

Hi Team:

             With the newly designed hardware, the signal amplitude received by the serial print photodiode is saturated, and the SIG_OVL_FLAG is 1. In addition, after the test, the photodiode is removed from PCBA, the received signal amplitude is saturated. In the data printed by the serial port, the temperature, ambient light and other data of OPT3101 can be read normally. What may be the cause of such a phenomenon

             This is a printout of the photodiode I removed:

             

             Thanks!!

  • Hi Pengsheng, 

    Could you please provide more details of the testing conditions? Which light source and photodiode are you using? What ambient light conditions? Which mode during the test? How many parts do you see the issue?

    Thank you.

    Wenjuan

  • Wenjuan,

           I tested using Auto HDR mode, and tested using OPT3101 Configurator Tool to generate configuration files;My test is to open the SDK INLAB_STEP_0 conditional compilation, serial print amplitude, phase, temperature and other data

           

           

           In the case of the photodiode, the amplitude data was saturated, so I removed the photodiode from the PCBA after testing, and the amplitude data read was still saturated;The photodiode I used was BPV22NF

           Using the same software, I was able to read the normal amplitude data using the OPT3101 EVM hardware

           The first time this happened!

           Thanks!!!!

           

  • Pengsheng,

    Thank you for the details.

    Could you let me know what calibrations have you done? Have you removed the crosstalk?

    Best regards,

    Wenjuan

  • Wenjuan

            Before the OPT3101 calibration, it is necessary to open conditional compilation INLAB_STEP_0, determine the calibration distance parameters according to the actual calibration target board and the amplitude value required for calibration, and write the calibration distance parameters into the refDistancesInMM array. However, the current phenomenon is that I open conditional compilation INLAB_STEP_0. Read the amplitude signal data is 65535, can not determine the calibration distance, can not calibrate, I will remove the receiving photodiode, read the amplitude signal data is still 65535, is my description clear, I can not carry out subsequent calibration under the current conditions, without receiving the photodiode in the case of amplitude data saturation may be what?

            Thanks!!!

  • Pengsheng, 

    I have some questions to help trouble shooting the saturation issue. 

    At what driver bias current do you see the issue? 

    Do you see the issue on one board or all the boards?

    Thank you.

    Wenjuan

  • Wenjuan,

          These are the driving currents I set up to test:

          

          

          

          The same phenomenon was found in all three PCBA tests!!

          After I removed the infrared emitting diode and receiving photodiode, the amplitude data printed by the serial port was still 65535

          This is the test I did,

          Thanks!!!

          

  • Pengsheng, 

    If you see the saturation issue even without emitting diode and photodiode, it is not due to light conditions. 

    Have you tried to test under low current setting, whether you will still see the issue?

    If the same issue is found on all the boards, we may need review the board layout. 

    Thank you.

    Wenjuan

  • Wenjuan,

       The test reduces the high and low threshold current of TX0 channel, the minimum is 2.8mA/1.4mA. The amplitude signal data printed by the serial port without receiving the photodiode is still 65,535 and saturated. Is this high probability caused by PCB layout?

       Thanks!

  • Pengsheng,

    Yes, I would suggest we need review the PCB layout. 

    Best regards,

    Wenjuan