This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMP275: TMP275 SDA/SCL under shoot Spec

Part Number: TMP275

Tool/software:

Hi Team

could TMP275 SDA/SCL afford such under shoot ~-0.5V like below?

BRs

Brian

  • Hi Brian,

    A slight undershoot is acceptable however, I would recommend mitigating this undershoot level since it is very close to absolute minimum spec from the datasheet (please see below). This could result in damage to the internal ESD structure of the device and cause permanent damage to it. Try adding a small series resistance to the communication lines to limit the amount of current that the bus drives.

    Best regards,

    Simon Rojas