This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMP91000: Wiring LMP91000 to SPEC Sensor

Part Number: LMP91000


Tool/software:

Hello,

I wanted to ask a question about the LMP91000 AFE. I have a SPEC Sensor like this one: Nitrogen-Dioxide-Sensor-110507_110508_110509_1.pdf (spec-sensors.com)

I saw that it has two working pins, can I wire them together so I can connect the sensor to the AFE?

Thank you very much for your help.

  • Juan,

    I'm not sure they can wired together. Do you think it's possible that they are duplicate pins, so two different AFEs could be connected, one to each working electrode? I would first try to see if they output the same current levels. We do have some recommendations on using a 4-lead chemical cell, but those usually have an "aux" pin as the 4th, not another working electrode pin.

    Regards

    -Alex Thompson

  • I think they are duplicated pins. I have asked the manufacturer of these sensors to check. I will update this thread as soon as I have answers