This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR2243: Porting mmwavelink to linux

Part Number: AWR2243

Tool/software:

Hi experts,

I am currently attempting to port  the mmwavelink API to a Linux based TDA4VEN. I hoped to use the mmwavelink_cascade_example acquired from the MMWAVE DFP 02.02.04.00. And i also learn the porting guide of the mmwaveLink framework.

The question is i am not quite sure how to implement communication interface callbacks, it seems that a Windows LIB file (mmwave_port_ethernet) has been included, but the source code for the platform implementations is not included, and there is no Linux lib.

Do I need to implement these interface functions myself?like the functions spiReadFromDevice, TDAcommopen. Are there any other reference available or lib provided to implement these interface in Linux system?

Best Regards,

Qiu