Tool/software:
Dear awr1432 expers,
I play and study the \MMWAVE_L_SDK_05_05_00_02\examples\mmw_demo\mmwave_demo and found out I can NOT set the SNR threshold to filter the weak object detection.
I try to set the SNR threshold use cfarCfg and cfarScndPassCfg commands in the profile as follows.
cfarCfg 2 4 3 2 0 12 1 0.5 0 1 0 0
cfarScndPassCfg 1 2 8 4 3 1 12 1
As the above, the Range CFAR and Doppler CFAR should filter out all detections SNR lower 12 dB.
However, that seems does not work at all.
Do I mis-understand the meaning of the parameters of cfarCfg and cfarScndPassCfg?
Help please.