This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMT87: RC Filter on remote ADC end & the Series Resistor on the Sensor end

Part Number: LMT87

Tool/software:

Hello E2E Team,

We are planning to use LMT87 for our remote temperature measurement use case with sensor being encapsulated inside a SS Metal Probe.

I want to understand for a CAT6 Twisted pair cable length of 6m from sensor to the ADC - followed by a RC based LPF filter on the ADC side with R=1kOhm or 100kOhm & C= 0.1uF or 1nF do we need to install a series resistor on the sensor side?

Assuming the Resistor of the RC Filter will act as the isolating/stability resistor & the effective C_Load that the LMT87 experiences is effectively only the cable capacitance of about 300pF which is far less than 1100pF limit as mentioned in the datasheet.

Kindly guide.

  • Also suggest a better RC Filter configuration for an effective cutoff of about 1kHz to 2kHz range.

    1. R: 1kOhm & C: 100nF
    2. R: 10kOhm & C: 10nF
    3. R: 100kOhm & C: 1nF

    Let me know which RC Filter configuration is better suited for the LMT8x series analog sensors.

  • Neet,

    If the cable capacitance is really only about 300pF, then you will not need the series resistor at the sensor side for stability, you are correct about that. I believe all of these options should be fine, you can go with option 1 if you really aren't sure.

    Thanks

    -Alex Thompson