Part Number: OPT3001-Q1
Tool/software:
Hi Team,
We are doing the continuously power on/off test of OPT3001-Q1. And we found that the CRF bit = '0' sometimes.
configure register = 0xC610

Below is our startup setup.
- RN[3:0] = 0x11
- CT = 0
- M[1:0] = 11
- POL = 1
We will check the CRF bit whether is '1' regularly.(25ms) If it reported '1', we will do the conversion.
But after multiple power on/off, CRF will remain '0'. Do we have wayto solve it like software reset?
Regards,
Roy