Tool/software:
Hello, I am working on a project to sense current in power transmission lines at distances of roughly 10m. I have the DRV425EVM and a high speed ADS. I expect the anomalous field intensity to vary between a few nT to a few hundred nT due to load imbalance in the transmission lines. I need to capture the 60Hz waveform and want to sample faster than 1kHz.
The EVM comes with a 100 ohm resistor, and the user manual suggests that increasing this will increase sensitivity and decrease max field. Will it also reduce noise density?
Also the datasheet for the senor itself quotes a 1.5/root(Hz) noise density. It is unclear if that is what I should expect using the EVM as it is factory configured. If not could you please explain what I should expect with factory EVM and what i could expect by changing the R1 resistor?
Thank you,
Noah