Part Number: IWR6843ISK
Other Parts Discussed in Thread: IWR6843,
Tool/software:
RS232 will not connect on the 6843ISK all the time. I have several 6843ISK boards. If I just use a USB cable to the board, and mmWave Studio, I have had cases where a board will not connect to the RS232. When that happens, it also won't work using the DCA1000 with the 6843. If I try enough times, suddenly it will connect. Then it continues to work and will work with the DCA1000. It seems like the USB ports that are identified follow the 6843 board. I just got a new IWR6843 board. It won't connect. With the switches identical, my old one will, but uses different USB port numbers. In fact, on the board that now works, it didn't work for many hours, then suddenly started working. I just kept plugging and unplugging the USB. Once it worked, it kept working. I have had this happen in the past. Very frustrating! Ideas????
Larry