Part Number: AWR1843AOPEVM
Other Parts Discussed in Thread: AWR1843AOP
Tool/software:
I am now implementing the AWR1843BOOST MRR demo using AWR1843AOP and would like to change USRR mode.
Please review the content below to see if there are any problems.
/* Tx antenna configuration in AWR1843AOP - USRR mode(2D mode only, NOT 3D mode) */
1.Almost all country - 79GHz Radar regulation:
Maximum radiated average power spectral density (e.i.r.p.) [dBm/MHz] of the EUT < -3 dBm/MHz
2.Calculation EIRP
One Tx at time: TX antenna feeding + Antenna Gain = 20mW + ~5dBi(AOP) = ~18dBm EIRP
Two Tx at time: One Tx + 3dB = ~21dBm EIRP
3. Conversion to radiated average power spectral density
[USRR30 occupied bandwidth = 2475MHz]
18dBm = ~ 64mW
21dBm = ~ 128mW
64mW/2475MHz = 0.02585858...
128mW/2475MHz = 0.05171717...
PSD(One Tx at USRR): 10log(0.02585858) = -15.8739dBm/MHz
PSD(Two Tx simultaneous at USRR): 10log(0.05171717) = -12.8636dBm/MHz
4.Check 79GHz EIRP regulation(below -3 dBm/MHz)
USRR two Tx Mode is OK
HK,Shin