The TI E2E™ design support forums will undergo maintenance from July 11 to July 13. If you need design support during this time, open a new support request with our customer support center.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR6843AOPEVM: Address mismatch between sys_common_xwr68xx_mss.h file & AWR6843AOPEVM DataSheet in (mmwave_sdk_03_06_02_00) SDK

Part Number: AWR6843AOPEVM
Other Parts Discussed in Thread: AWR6843AOP

Tool/software:

Hello Team,

I'm referring mmwave_sdk_03_06_02_00-LTS, In that the header file "sys_common_xwr68xx_mss.h" contains macros that specify the base addresses. Is the AWR6843AOPEVM model associated with those addresses?

While checking "UART_config" in the UART_init() function, I was unable find these addresses in the "AWR6843AOP Single-Chip 60- to 64-GHz mmWave Sensor Antennas-On-Package (AOP)" datasheet.

  • Hey Shubham,

    Yes, the addresses within the sys_common_xwr68xx_mss.h are also applicable for AWR6843AOPEVM.

    While checking "UART_config" in the UART_init() function, I was unable find these addresses in the "AWR6843AOP Single-Chip 60- to 64-GHz mmWave Sensor Antennas-On-Package (AOP)" datasheet.

    I'm a bit confused on why you are looking for an address that is associated with UART_config. UART_config is an array of structs that each contains a function table, driver data object, and hardware attribute structure. UART_init will call the init function registered in the UART_config function table, UartSci_init, which effectively does nothing. UartSci_open is where most of the configuration for each UART peripheral is handled.

    Anyways, I just wanted to provide some extra context to the UART driver, but let me know if this answered your question.

    Regards,

    Kristien