This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1843AOP: AWR1843AOP

Part Number: AWR1843AOP
Other Parts Discussed in Thread: LP87524B-Q1

Tool/software:

AWR_PMIC_question.pptx

For AWR1843AOP - PMIC low noise application:

I read TI two materials(Power Management Optimizations & PMIC datasheet) that reduce noise using LDO.

I would like to clearly know the initial OTP setting voltage value of LP87524BRNFRQ1 when I do not set it's value using I2C.

This is to reduce power consumption as much as possible.

Q1) LP87524BRNFRQ1 -> Buck2 OTP default voltage setting: 1.8V or 1.3V >> 1.3V?

Q2) LP87524BRNFRQ1 -> Buck3 OTP default voltage setting: 2.3V or 2.1V >> 2.1V?

Thanks,

HK,Shin