Other Parts Discussed in Thread: AWR2944EVM, LM76003, LM63635-Q1
Tool/software:
When I use the AWR1843AOP considering truck/bus radar, the power supply must be configured to a maximum input of 29V typical and 60V transient.
Therefore, looking at the AWR2944EVM material, I understand that the PMIC uses a switching frequency outside the IF band, so there is no need to use multiple external LDO.
There is no suitable DCDC IC for the first input stage, but according to TI data, the DCDC (LM76003) IC for 60V switches at 400~500KHz due to heat generation.
(Q1) If I use LM76003(1st regulator) at switching frequency 500KHz, please be sure there is no effect on the ripple voltage(AWR1843AOP) required by the radar 1.0V or 1.8V power supply.
(Q2) When I use LP877451A1RXVRQ1 same as AWR2944EVM, the default setting value(1.0V/1.2V/1.8V/3.3VIO/5V) is not any problem?(I want to use SPI bus off state)