This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV401-Q1:no

Part Number: DRV401-Q1
Other Parts Discussed in Thread: DRV401

Tool/software:

您好、我想询问 drv401是否具有过温保护功能、最高工作温度是多少?如果在应用过程中没有添加超温保护电路?

  • Hello,

    From your question translated: Hi, I would like to ask if the drv401 has an over temperature protection and what is the maximum operating temperature? If no over temperature protection circuit has been added during the application?

    The DRV401 does not have over temperature protection.  The temperature limitations are on the datasheet.

    Max operating temperature: 150°C

    Max temperature for operating specifications:125°C

    Regards,

    Javier