Tool/software:
Hi,
I read another conversation related to my question in this link:
the datasheet of AWR1843 mentioned these two sentences in page 29 of it:
- "Less than ±0.5 dB pass-band ripple/droop"
- "Better than 60 dB anti-aliasing attenuation for any frequency that can alias back into the pass-band."
Cesar mentioned in conversation of above link, "These parameters are related to the digital baseband and not the HPF.".I'm confused about this. Anti-aliasing filter should be before ADC and couldn't be after ADC and in digital chain. Because it should reduce low ADC Rate effects that make aliasing. So Anti-aliasing filter should be before ADC in order to reduce frequencies more than 0.5*ADC Rate (Nyquist).
please Help me.
Thanks