This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV5055-5057EVM: Is there a sensor module that uses only the DRV5056?

Part Number: DRV5055-5057EVM
Other Parts Discussed in Thread: DRV5056, DRV5057, , DRV5055

Tool/software:

I am looking for a Hall effect sensor module to measure the displacement of a vibrating component. However, the DRV5055-5057EVM includes all three sensor types (DRV5055, DRV5056, and DRV5057), making it too large for my application.

Is there a smaller sensor module that uses only the DRV5056? If not, do you have any recommendations for a compact alternative?

  • Hi Minhyeong,

    Thank you for posting to the Sensors forum!

    If you are looking for a smaller EVM to evaluate the DRV5056, one option that you can do is get the HALL-ADAPTER-EVM. The HALL-ADAPTER-EVM is a breakout board that has a bunch of different package options available, including one for the DRV5056 (SOT-23/TO-92). All you would need to do is get the DRV5056 device and populate it on the corresponding breakout board.

    Best,

    ~Alicia