Hi everyone,
Recently, I tried configuring the OPT3101 sensor into Dealias Mode for long-distance measurements. However, I'm encountering an issue where the output signal on the LED pin is extremely weak — it's only detectable up to about 10 cm , which is way below the expected performance.
I've configured all the registers according to the official TI Dealias mode documentation , and also referred to community solutions such as this one (https://e2e.ti.com/support/sensors-group/sensors/f/sensors-forum/1345290/opt3101-dealias-mode) . Unfortunately, none of these suggestions resolved the issue.
Out of curiosity, I tried disabling the sequencer mode , so that the device doesn't automatically switch frequencies. That’s when I started getting a normal signal output. However, this approach obviously doesn’t run in Dealias Mode , so it's not a real solution.
So now I’m wondering:
- Is there a way to manually switch between frequencies in Dealias Mode instead of relying on the sequencer?
- Or can I configure the sequencer to switch more slowly between frequency steps?
- Are there any other known issues or configuration tips related to enabling Dealias Mode successfully?
Any advice or insights would be greatly appreciated!
Thanks in advance!