This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DCA1000EVM: IWRL6432AOP : FTDI problem

Part Number: DCA1000EVM
Other Parts Discussed in Thread: IWRL6432AOP

Tool/software:



Hi, I installed FTDI using \ti\mmwave_studio_04_01_00_06\ftdi\dpinst64.exe.
However, I can only see the two ports below, and the top four ports are not visible.
I am using the IWRL6432AOP and DCA1000EVM.

Does the D10 LED on the IWRL6432AOP turn on when the top four ports are connected?
Also, is it possible to perform data capture even if the four COM ports are not visible?


Do all the connection statuses on the mmWave Studio GUI need to show "Connected" in order to perform data capture?
Or, for data capture, which specific parts or connections are required to be successfully established?

I will wait for your response. Thank you.