This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV5056: Behavior when Vout < Vq=0.6V

Part Number: DRV5056
Other Parts Discussed in Thread: DRV5055

Tool/software:

I am working on a product (call it "A") that is using the DRV5056Z1QDBZR sensor, with Vcc=5V. The sensor senses a magnet in a mating product (call it "B"). When "B" is not mated, the sensor output is about 0.6V as expected. When "B" is mated the sensor output is about 0.9V, corresponding to about 1.5mT of flux density. Unfortunately, it turns out that the assembly SOP of "B" did not control for the magnet polarity. What I see is that when some units of "B" are mated, the sensor output is about 0.3V. I have not verified but I assume the flux density seen at the sensor for the reverse polarity units is "-1.5mT" (or 1.5mT in the "NORTH" polarity). I would like to be able to rely on the output voltage of any mated unit of "B" to be either 0.9V or 0.3V. I see that the datasheet for DRV5056Z1QDBZR says that any output below Vq~=0.6 results in non-linear behavior. This is fine as long as it is repeatable. I am hoping someone from TI can confirm the repeatability of DRV5056Z1QDBZR when there is a NORTH field present and Vout is about 0.3V.

I know that the DRV5055 offers bipolar linearity. However, the DRV5056Z1's sensitivity of 200mV/mT is important for this application. So, I would like to stick with the DRV5056Z1.

  • Hi Sage,

    Our team is out today.  We should be able to take a look at your question when we are back in the office starting tomorrow.

    Regards,

    Mekre

  • Hello Sage,

    I spoke with one of our validation engineers about this and he mentioned that he observed non linearity closer to outputs at or below 0.1V.  That being said, his sample set is likely less than 100 units and we do not guarantee behavior outside of our specified sensing range.  Within a sample lot and narrow operating temperature range the probability of repeatable behavior is higher.  However, if you are building large volumes with multiple lots and the device is expected to operate at different temperature extremes, the repeatability may not be as good as desired.