This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPT3101: Frequency Calibration with external reference clock

Part Number: OPT3101


Tool/software:

Hi,

I am trying to implement the external frequency calibration into my calibration script ( as per OPT3101 Distance Sensor System Calibration (sbau310)).

Custom Hardware.

Opt runs fine without ext freq calib, trying for more precision.

Trimmed frequency works as expected, however setting EN_AUTO_FREQ_COUNT =1 tanks my measured phase (_H = 5, _L = 7) and the calibration is void.

My ext clock runs at 32789 +- 0.140 Hz

REF_COUNT_LIMIT=19518

SYS_CLK_DIVIDER=10

On another note, what order is required for setting the various frequency calibration register? Is there a required timing to set START_FREQ_CALIB = 0, or should i leave this high?

Appreciate the help.

Regards, Josh

  • Hi Josh,

    Are all registers required for external freq cal getting set?

    Here is some example initialization sequence 

    Here is all registers related to this calibration

    For this question: On another note, what order is required for setting the various frequency calibration register? Is there a required timing to set START_FREQ_CALIB = 0, or should i leave this high? - see the initialization sequence example above. One key item will be setting these settings before starting the device (TG_EN=1) as shown in the sequence.

    Best,

    Alex

  • Hi Josh,

    Since some time has passed, marking this closed for now - please let us know if further help needed

    Best,

    Alex