Other Parts Discussed in Thread: IWRL1432, , IWR1642
Tool/software:
Hello,
I would like to inquire about the maximum number of ADC samples supported by the following modules: IWRL1432, IWR1443, and IWR1642.
(This is to determine the maximum sample configuration for future signal processing with the DCA1000.)
I adjusted the parameters using the mmWave Sensing Estimator (v2.4.0). (https://dev.ti.com/gallery/view/mmwave/mmWaveSensingEstimator/ver/2.4.0/)
For the IWRL1432, when I set numOfAdcSamples beyond 2048, a warning message is displayed:
"% numOfAdcSamples must be between 2 to 2048".
However, for the IWR1443 and IWR1642, even when setting numOfAdcSamples to 4096 or 8192, no warning messages appear.
In this case, does it mean that for IWR1443 and IWR1642, as long as there is no error in the mmWave Sensing Estimator output, we can assume that numOfAdcSamples values like 4096 and 8192 are valid and usable?
I look forward to your clarification.
Thank you.