Part Number: TMCS1126-Q1
Tool/software:
Hi TMCS1126-Q1 I have a question
If you look at the TMCS1126-Q1 application note, use L5, C7 when VREF is output to the outside, we have 20nF for VREF, we use resistance voltage distribution to create VOC, and the circuit is configured only inside without outputting outside
Q1. Is it necessary to apply L5 and C7 even when I don't take out VREF pins to the outside?
Q2. If you look at the application notes, I connected the VOC with VS, but in what case should I connect it?