This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR2E44PEVM: rlSetSubFrameStart return the error code : RL_RET_CODE_FRAME_ALREADY_ENDED

Part Number: AWR2E44PEVM


Tool/software:

Hello Expert,

Sometimes, rlSetSubFrameStart return the error code(RL_RET_CODE_FRAME_ALREADY_ENDED) . The error rate is approx. 3%.

What triggers the RL_RET_CODE_FRAME_ALREADY_ENDED error? Why is RL_RET_CODE_FRAME_ALREADY_ENDED?

If we add 250us delay after rlSensorStart, the error no longer occurs during a ​​1-hour continuous test. I don't find the requirement for delay between rlSensorStart and rlSetSubFrameStart from mmWave-Radar-Interface-Control.pdf.  I am certain that the previous frame is end, so i don't kown why 250us delay is useful for this error.

Can you explain this test result?

The SDK version is mmwave_mcuplus_sdk_04_07_01_01 and dfp version is mmwave_dfp_02_04_17_01.

Regard,

Bin