This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSS4470: TUSS4470 with Linux

Part Number: TUSS4470


Tool/software:

Hi, 

I am trying to interface the TUSS4470 with i.MX93 via SPI ports.

I tested the SPI in loopback and logic, the SPI configuration is ok, and it was also confirmed by the i.MX93 vendor.

I want to read the TUSS4470 chip ID, hence register 0x1D, and I send the following command from tthe erminal:
spidev_test -D /dev/spidev0.0 -s 500000 -b 8 -H -p '\xBA\x00'
-v
spi mode: 0x1
bits per word: 8
max speed: 500000 Hz (500 kHz)
TX | BA 00 __ __ __ __ __ __ __ __ __ __ __ __ __ __ __ __ __ __ __ __ __ __ __ __ __ __ __ __ __ __ |..|
RX | 00 00 __ __ __ __ __ __ __ __ __ __ __ __ __ __ __ __ __ __ __ __ __ __ __ __ __ __ __ __ __ __ |..|

I always received 00 00, but in the logic it seems that the TUSS answered with 00 B9.

Any advice? 

BR
Basel