Part Number: AWR1843BOOST
Tool/software:
AWR1843BOOST OOB Demo – Range drops when ego vehicle is moving
Hi,
I'm using the AWR1843BOOST with the Out of Box demo. While testing on a moving vehicle, I'm seeing that the detection range drops from ~45 m (when stationary) to ~20–25 m.
I expected around 70 m range based on the Sensing Estimator(screenshot is attached below). Lowering the SNR threshold improves range (up to 65 m), but adds a lot of noise.below i added my config also
Why does range drop while moving?
Is this due to velocity resolution, or motion-related SNR degradation?
What config parameters (e.g., CFAR, threshold) should I tune to fix this?
Thanks,
Sandeep