Part Number: DRV5055-Q1
Tool/software:
Hello here smart people,
we are currently working with the DRV5055-Q1 hall sensors for the detection of a ISO26262 safety relevant lock position. For this we are doing a error analysis on the possible output voltages where we summed of the tolerances of the DRV5055-Q1's datasheet up to 5%. Is this a realistic error to assume or do you have some measurements for this sensor available, showing the standard error distribution on the DRV5055-Q1 outputs gair and offsets or the error on the production batches?
best regards