Tool/software:
Hello team,
I am estimating the impact of errors on Vout and would like to ask the following question regarding PSRR:
- When PSRR [A/V] multiplied by device sensitivity, can it be output-referred parameter?
- Is "Reference Output Voltage PSRR" independent of the Vout deviation stated as "Reference Output Voltage" in the datasheet?
- Are the Integrated Reference characteristics common between "Vref" which be added to Vout and "VREFout"?
- Based on the equation "Vout = (Iin × S) + Vref, is my understanding correct that PSRR and Reference Output Voltage PSRR are independent?
- I understand that the purpose of the "Vref output" is to eliminate offset errors introduced at the system level. Without it, cannot errors caused by power supply fluctuations be canceled out, even if the CPU (ADC) shares a common power line?
Best Regards,
Akira