This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWRL6844EVM: AWRL6844EVM

Part Number: AWRL6844EVM
Other Parts Discussed in Thread: AWRL6844

Tool/software:

Hi, currently i am trying to set up the AWRL6844 EVM demo board using the DCA1000 data capture guide provided, until now i was following it step-by-step, but all of a sudden the PGOOD and the RESET_LED stopped blinking, and the software throws an error while trying to run the script provided.

I am ESD protected, but still can't figure out what could have caused this. The only blinking led is the D6 which indicates that the board is connected to a power supply.

Is there any way to diagnose if it was a short somewhere or read out the state of the board from the software?