Tool/software:
Hi,
We use the HDC2010 for the temperature and humidity collection,
and now, The SMT processing factory will first help us mount the hygrometer onto the PCB.
After returning, we will conduct random humidity measurement by setting the temperature to 25C and the humidity to 30%, 50%, and 70% respectively in the test box.
The readings of the hygrometer on the PCBA will be compared with our standard source Rosennik hygrometer. If the error exceeds our standard, it will be judged as unqualified.
We find there are much more test data is not qualified, please refer to below test data form, and “fail“ is unqualified;
PGS4000-V3.0 20250716(4).xlsxPGS4000-V3.0 20250627(1).xlsx
Below is our schematic diagram:
The below is our I2C configuration:
1. The below is Humidity value analysis:
2. The below is temperature value analysis:
3. Please review our schematic diagram and I2C configuration, and advise that how to improve our design for this case, thanks.