This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AFE3010: Help Required using AFE3010

Part Number: AFE3010


Tool/software:

Hi,

I have designed and using the following circuit for 220V 50Hz:

The issue that I am facing that the self test is not being passed and I am getting 1.2 sec pulses on the ALARM pin. There is no effect on the self test if the CT is connected or not. The CTs that I am using are ZST065BT with turns ratio of 1000/1 and 200/1. How to debug the situation?