Tool/software:
Question one:If HSM core has registered the interrupt HSM_MBOX_READ_ACK
, which register should be configured to enter the ACK interrupt handler function in the Secure host R5F core?
Question two:In the SDK package (tifs_awr294x_10_01_00_01
), I couldn’t find the register R5FSS0_0_MBOX_READ_DONE_ACK
shown in Figure 1 in the chip manual,Can you give me help?
picture 1