This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR2944PEVM: Antenna redesign with 4-RX elevation array and azimuth-steered TX – need confirmation on 5 steering control items

Part Number: AWR2944PEVM


Tool/software:

Hi TI team,

We are redesigning the antenna on the AWR2944PEVM to use the device’s RF front end in a hybrid configuration:

  • Four RX channels form a fixed elevation multibeam curtain (passive receive, no switching).

  • One TX chain performs analog azimuth beam steering across ±15°, updated once per frame (CPI = 60 ms or 120 ms).

Before finalizing the antenna hardware and calibration plan, we need confirmation on the following five control-interface points:

  1. Atomic phase and amplitude commit at frame boundary
    Can all TX elements update phase and amplitude together using shadow registers with a single frame-sync latch?
    What are the effective phase resolution, INL/DNL, and temperature drift limits?
    Acceptance: atomic commit; combined pointing error (quantization + drift) ≤ 0.3–0.5° rms over ±15°.

  2. Beam squint across FMCW sweep
    What is the maximum azimuth squint at ±15° across the typical chirp bandwidth?
    Are sub-band steering tables or compensation methods supported?
    Acceptance: squint < ⅓ beamwidth or mitigation available.

  3. Per-steer calibration LUTs (phase and amplitude)
    How can per-steer phase and amplitude LUTs (including tapers) be preloaded?
    What is the bank size, number of banks, and swap time per frame?
    Acceptance: ≥ 256 entries per bank or fast bank swap; ≤ 10 µs index-swap; background reload supported.

  4. Amplitude taper capability
    What bit-depth and dynamic range are available?
    Can amplitude values latch atomically with phase at frame-sync?
    Acceptance: ≥ 7–8 bits, ≥ 10–12 dB range, same commit timing as phase, glitch-free.

  5. Multi-device synchronization (if cascaded)
    Is there PPS/10 MHz support, guaranteed frame-start skew, and a method to phase-align multiple devices so all commit the same beam index simultaneously?
    Acceptance: < 50 ns frame-start skew; documented phase-align; same-frame commit supported.

References to datasheet sections or example threads would be greatly appreciated. Thank you!