Other Parts Discussed in Thread: ADC088S052, TMP61
I want the Digital value for the temperature having 19 degree and 23 degree celcius and 29 degree celcius and our ambient temperature is 22 degree celcius. what will be the we are using biasing voltage 3.3V and Rbias 10K and having 8 bit ADC ADC088S052 which is sensing analog voltage of thermistor. Please help in this regard. I want to map exact digital values and also tell is there any error in adc or thermistor that needs to be cleared.? And how to check it . Can you please what and how we can make test setup to measure all this and get thermistor resistance vs temperature reading for every resistance. And is there way of approximating digital counts or exact one value . Thermistor we are using is TMP6131LPGM.And for mappping any Excel sheet available please provide for direct calculation
Thanks & Regards
Nishant Gupta