This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWRL6432: IWRL6432 SYNC_IN with delayed frame trigger

Part Number: IWRL6432


Hi.

I am using an IWRL6432. I want to use the SYNC_IN pin to trigger frames. As far as I can see, it is possible to use the FrameTrigMode to HW_LOW_JIT_TRIG. image.png

However, according to the datasheet, I can set a delay for the frame start. image.png

This is visualized here:

image.png

However, I am not able to find the delay in the source code or configuration. Can you help me find it in the source code?

My application uses two sensor with an overlap, so I need to delay one of the sensors, to avoid ghost points.

Thank you in advance.