Hello,
I am using the FDC2214 device for a liquid level measurement application. I am operating two channels of the device (CH0 and CH1) to measure the liquid levels in two separate containers. When I run a single channel, the system operates without any issues; however, when both channels are enabled simultaneously, the data ready flag stops being asserted after approximately 5–10 seconds. In this condition, even if the liquid level changes, I cannot receive data from either channel.
I initially suspected that the issue might be caused by a long conversion time, so I modified the RCOUNT and SETTLECOUNT values, but the problem persisted. I then configured different IDRIVE values for the channels, and with this adjustment, the time before the issue appears increased to around 30 minutes.
What could be the root cause of this behavior? Any guidance or support on this issue would be appreciated.