This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPT3001: Clarification required on OPT5001

Part Number: OPT3001
Other Parts Discussed in Thread: OPT5001

Hi,

TI part number is selected as OPT3001 as there is no selection available for OPT5001.

Kindly clarify the below queries regarding opt5001.

  1. INT pin shall toggle to indicate the result ready state. when the INT pin toggle back to the other state?
  2. why fullscale mantissa value is different for secondary conversion though the conversion time is same
  3. why DIV_FACTOR is not available for dual edge conversion
  4. what is the difference in AGC enabling for all conversions or first conversion alone. what is the benifit in using for first conversion alone.
  5. EN_HIGH_CONV_TIMES register parameter is confusing - description is conflicting with parameter range value description. Also pls brief how this affects the result value?
  6. parmeters CFG_RANGE_1, CFG_RANGE_0 - to be configured when AGC is ON or OFF?
    what is offset calibration?